:FUNCtion:XSCale
Command Syntax
:FUNCtionN:XSCale <seconds>
<seconds> is a double.
Where N identifies one of sixty four {1:64} math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtionN:XSCale?
Description
Sets the horizontal time scale in seconds-per-division or symbols, depending on the timebase units setting (:FUNCtion:XUNits?). Use the :FUNCtion:XPOSition to set the horizontal position ( time delay relative to the trigger event). Use the :FUNCtion:XLEFt? to query the time value at the graticule's left edge and :FUNCtion:XRIGht? to query the time value at the graticule's right edge.