:HISTogram:ASCii:DATA?

Query Syntax

:HISTogramN:ASCii:DATA?

Where N identifies one of four possible histograms {1:4} that you can design. For example, :HISTogram3.

Description

Returns the histogram database as ASCII data (comma-separated values). Each value provides the number of counts for each point in the histogram. To query the number of points (comma-separated values), use the :HISTogram:POINts? query. To return the data in binary, use the :HISTogram:INTeger:DATA? query.