:HISTogram:WINDow:BORDer
Command Syntax
:HISTogramN:WINDow:BORDer {ON | OFF | 1 | 0}
Where N identifies one of four possible histograms {1:4} that you can design. For example, :HISTogram3.
Query Syntax
:HISTogramN:WINDow:BORDer?
Query Response
{1 | 0}
Description
Displays (ON) or hides (OFF) the solid-line histogram window border. The border allows you to view which region of the measurement database is used to construct the histogram. The border does not have to be displayed to create a histogram. By default, the border is off. The histogram must be enabled prior to enabling the histogram window border.