:HISTogram:SOURce

Command Syntax

:HISTogramN:SOURce  <source_waveform>

Where N identifies one of four possible histograms {1:4} that you can design. For example, :HISTogram3.

Where <source_waveform> can be one of the following:

  • CHANnel<connection1-8>_<ch1-8>; With connection 1, the "1_" part is optional, and you can simply use CHANnel<ch1-8>.
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:64}

Query Syntax

:HISTogramN:SOURce?

Description

Selects the source waveform for the indicated histogram. The histogram window will track the source's vertical and horizontal scale.