:HISTogram:POINts?

Query Syntax

:HISTogramN:POINts?

Where N identifies one of four possible histograms {1:4} that you can design. For example, :HISTogram3.

Description

Queries the number of points in the histogram. For vertical (left and right) histograms, this is the number of points along the vertical axis. For horizontal (top and bottom) histograms, this is the number of points along the horizontal axis. Use the :HISTogram:INCRement? query to return the amplitude or time spacing between the points. To return the actual counts for each point, use the :HISTogram:ASCii:DATA? or :HISTogram:INTeger:DATA? queries.

Vertical Histogram (LEFT)

Horizontal Histogram (BOTTom)

More Information