:HISTogram:INCRement?
Query Syntax
:HISTogramN:INCRement?
Where N identifies one of four possible histograms {1:4} that you can design. For example, :HISTogram3.
Description
Queries the amplitude or time spacing between the points in the histogram. For vertical (left and right) histograms, this is the amplitude spacing between the points are along the vertical axis. For horizontal (top and bottom) histograms, this is the time spacing between the points along the horizontal axis. Use the :HISTogram:POINts? query to return the number of points in the histogram. To return the actual counts for each point, use the :HISTogram:ASCii:DATA? or :HISTogram:INTeger:DATA? queries.
Vertical Histogram (LEFT)
Horizontal Histogram (BOTTom)