:HISTogram:SCALe
Command Syntax
:HISTogramN:SCALe {LINear | LOG}
Where N identifies one of four possible histograms {1:4} that you can design. For example, :HISTogram3.
Query Syntax
:HISTogramN:SCALe?
Description
Sets the selected histogram's scale to linear or logarithmic. The default setting is LINear.