:LTESt:MEASure:MLIMit:FREGion
Command Syntax
:LTESt:MEASure:MLIMitN:FREGion {INSide | OUTSide}
Where N identifies one of sixteen {1:16} limit tests.
Query Syntax
:LTESt:MEASure:MLIMitN:FREGion?
Description
Defines when to fail a measurement limit test. Use one of the following arguments:
- INSide
- A measurement is counted as a failure if it is within the lower and upper limits, which are set by the
:LTESt:MEASure:MLIMit:LLIMitand:LTESt:MEASure:MLIMit:ULIMitsibling commands. - OUTSide
- A measurement is counted as a failure when the measurement results exceed the parameters set by
:LTESt:MEASure:MLIMit:LLIMitand:LTESt:MEASure:MLIMit:ULIMitsibling commands
Use the :LTESt:MEASure:MLIMit:STATe sibling command to start the limit test.
Example
:LTESt:MEASure:MLIMit2:FREGion INSide // Limit test 2 fails for inside violations.