:LTESt:MEASure:MLIMit:STATe
Command Syntax
:LTESt:MEASure:MLIMitN:STATe {ON | OFF}
Where N identifies one of sixteen {1:16} limit tests. For example, :MLIMit8.
Query Syntax
:LTESt:MEASure:MLIMitN:STATe?
Description
Turns the specified measurement limit test, 1 through 16, on or off. Source waveforms include channels, differential channels, and functions. Use the following sibling commands to configure the limit test:
:LTESt:MEASure:MLIMit:SOURce:TYPEselects the type of measurement.:LTESt:MEASure:MLIMit:SOURce:LOCationselects the actual measurement.:LTESt:MEASure:MLIMit:FREGionselects when to fail a measurement.:LTESt:MEASure:MLIMit:LLIMitdefines the lower limit for failing a measurement.:LTESt:MEASure:MLIMit:ULIMitdefines the upper limit for failing a measurement.:LTESt:MEASure:MLIMit:UPACtionselects an action if the measurement cannot be performed.
As seen in the example in this topic, the following commands configure the reports of a completed limit test:
:LTESt:MEASure:SIMage:STATe:LTESt:MEASure:SWAVeform:CHANnel{N}:STATe:LTESt:MEASure:SWAVeform:DIFF{N}:STATe:LTESt:MEASure:SWAVeform:FUNCtion{N}:STATe
Example Command Sequence
The following example creates three measurement limit tests for the Crossing %, Fall Time, and Rise Time measurements shown in this picture. Notice that the reporting action commands for saving waveform, summary, and a screen capture apply to all active measurement limit tests. The first limit test to complete stops all tests and report actions are taken.
:ACQuire:SINGle // Stop waveform acquisition.// CREATE MEASUREMENT LIMIT TEST 4. :LTESt:MEASure:MLIMit4:SOURce:LOCation 1 // Create test 4 for Crossing % measurement. :LTESt:MEASure:MLIMit4:LLIMit 23E-12 // 23 ps lower limit. :LTESt:MEASure:MLIMit4:ULIMit 24E-12 // 24 ps upper limit. :LTESt:MEASure:MLIMit4:FREGion OUTSide // Fail counted if outside of limit. :LTESt:MEASure:MLIMit4:UPACtion FAIL // If unable to perform test, fail. :LTESt:MEASure:MLIMit4:STATe ON // Turn Crossing % test on.// CREATE MEASUREMENT LIMIT TEST 5. :LTESt:MEASure:MLIMit5:SOURce:LOCation 2 // Create test 5 for Fall Time measurement. :LTESt:MEASure:MLIMit5:LLIMit 23E-12 // 23 ps lower limit. :LTESt:MEASure:MLIMit5:ULIMit 24E-12 // 24 ps upper limit. :LTESt:MEASure:MLIMit5:FREGion OUTSide // Fail counted if outside of limit. :LTESt:MEASure:MLIMit5:UPACtion FAIL // If unable to perform test, fail. :LTESt:MEASure:MLIMit5:STATe ON // Turn Fall Time test on.// CREATE MEASUREMENT LIMIT TEST 6. :LTESt:MEASure:MLIMit6:SOURce:LOCation 3 // Create test 6 for Rise Time measurement. :LTESt:MEASure:MLIMit6:LLIMit 23E-12 // 23 ps lower limit. :LTESt:MEASure:MLIMit6:ULIMit 24E-12 // 24 ps upper limit. :LTESt:MEASure:MLIMit6:FREGion OUTSide // Fail counted if outside of limit. :LTESt:MEASure:MLIMit6:UPACtion FAIL // If unable to perform test, fail. :LTESt:MEASure:MLIMit6:STATe ON // Turn Rise Time test on.// CONFIGURE REPORTING FOR ALL 3 TESTS. :LTESt:MEASure:SWAVeform:CHANnel2_1:STATe DISK // Save channel 2A data to file. :LTESt:MEASure:SWAVeform:CHANnel2_1:WMEMory WMEMory3 // Select memory 3. :LTESt:MEASure:SIMage:STATe ON // Save screen image file.// START TESTING. :ACQuire:RUN // Start waveform acquisition. *OPC? // Wait for completion of tests.