:LTESt:MEASure:MLIMit:SOFailure
Command Syntax
:LTESt:MEASure:MLIMitN:SOFailure {ON | OFF}
Where N identifies one of sixteen {1:16} limit tests. For example, :MLIMit8.
Query Syntax
:LTESt:MEASure:MLIMitN:SOFailure?
Query Response
{1 | 0}
Description
This command specifies whether measurement limit failures will cause acquisitions to stop.
When the measurement whose limits are being tested is measuring all occurrences within an acquisition, multiple measurements can be made per acquisition, and within those measurements, multiple can have limit failures. This means an acquisition that causes a stop can show multiple failures.