:MEASure:EYE:CONTour:DISPlay

Command Syntax

:MEASure:EYE:CONTourN:DISPlay {ON | OFF}

Where N identifies a group of contour lines and must be {1:16}.

Query Syntax

:MEASure:EYE:CONTourN:DISPlay?

Description

Displays (ON) or hides (OFF) the selected group of eye contour lines. Hiding an eye contour group does not delete the group. You can redisplay the group and even move it to another waveform. To move the group of eye contour lines, use the :MEASure:EYE:CONTour:SOURce command. To define the group's lines, use the :MEASure:EYE:CONTour:BERates command.