:MEASure:EYE:CONTour:RJSValue:EYE
Command Syntax
:MEASure:EYE:CONTourN:RJSValue:EYE{0:2} <random_jitter>
Where N identifies a group of contour lines and must be {1:16}. <random_jitter> is a double.
Query Syntax
:MEASure:EYE:CONTourN:RJSValue:EYE{0|1|2}?
Description
For Random Jitter (RJ) stabilization, sets the value of RJ for the selected eye of an eye-contour group. To measure the RJ, measure the RJ while using a signal that has a short pattern. Or, measure the RJ using a separate instrument, such as a spectrum analyzer. Use the :MEASure:EYE:CONTour:RJSTabilize command to turn on or off the use of RJ stabilization.
| Command | Description | |
|---|---|---|
| :EYEl2 | Applies to eye 2/3. |
|
| :EYE1 (or :EYE) |
Applies to eye 1/2. | |
| :EYE0 | Applies to eye 0/1. | |