:MEASure:EYE:CONTour:RJSTabilize
Command Syntax
:MEASure:EYE:CONTourN:RJSTabilize {ON | OFF}
Where N identifies a group of contour lines and must be {1:16}.
Query Syntax
:MEASure:EYE:CONTourN:RJSTabilize?
Description
Turns on or off Random Jitter (RJ) stabilization for a group of eye-contour lines. When RJ stabilization is on, use the :MEASure:EYE:CONTour:RJSValue:EYE command to enter a separate value of RJ for each eye. To measure the RJ, measure the RJ while using a signal that has a short pattern. Or, measure the RJ using a separate instrument. Each eye-contour line group has its own RJ stabilization values.