:MEASure:EYE:CONTour:PSPec

Command Syntax

:MEASure:EYE:CONTourN:PSPec {BER | PROBability}

Where N identifies a group of contour lines and must be {1:16}.

Query Syntax

:MEASure:EYE:CONTourN:PSPec?

Description

Selects eye contour lines based on BER or probability. To enter the values for each line, use the :MEASure:EYE:CONTour:BERates command. Selecting BER indicates Bit Error Rate for NRZ signals and Symbol Error Rate (SER) for PAM signals.