:MEASure:EYE:CONTour:RNSTabilize

Command Syntax

:MEASure:EYE:CONTourN:RNSTabilize {ON | OFF}

Where N identifies a group of contour lines and must be {1:16}.

Query Syntax

:MEASure:EYE:CONTourN:RNSTabilize?

Description

Turns on or off Random Noise (RN) stabilization for a group of eye-contour lines. When RN stabilization is on, use the :MEASure:EYE:CONTour:RNSValue:LEVel command to enter a separate value of RN for each eye level. To measure the RN, measure the RN while using a signal that has a short pattern. Or, measure the RN using a separate instrument. Each eye-contour line group has its own RN stabilization values.