:MEASure:JITTer:NOISe:ERNValue:LEVel
Command Syntax
:MEASure:JITTerN:NOISe:ERNValue:LEVel{0:1} <stable_RN_value>
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
<stable_RN_value> is a double.
Query Syntax
:MEASure:JITTerN:NOISe:ERNValue:LEVel{0:1}?
Description
When user-defined values for RN compensation have been enabled (see :MEASure:JITTer:NOISe:RNComp) and explicit clock recovery is being used (see :CRECovery:MODE or :<source>:CRECovery:MODE), this command lets you specify the appropriate RN values for the explicit clock symbol levels.