:MEASure:JITTer:NOISe:RNSValue:LEVel

Command Syntax

:MEASure:JITTerN:NOISe:RNSValue:LEVel{0:1} <stable_RN_value>

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

<stable_RN_value> is a double.

Query Syntax

:MEASure:JITTerN:NOISe:RNSValue:LEVel{0:1}?

Description

When using RN stabilization (see :MEASure:JITTer:NOISe:RNSTabilize), this command lets you specify the appropriate RN values for the symbol levels.