:MEASure:JITTer:NOISe:MLOCation
Command Syntax
:MEASure:JITTerN:NOISe:MLOCation <pct_of_bit>
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
<pct_of_bit> is a double.
Query Syntax
:MEASure:JITTerN:NOISe:MLOCation?
Description
This command specifies the measurement location within the bit where 0% is the beginning of the bit, 50% is the middle of the bit, and 100% is the end of the bit.
You can specify a location value from 5% to 95%.