:MEASure:JITTer:NOISe:RNCValue:LEVel
Command Syntax
:MEASure:JITTerN:NOISe:RNCValue:LEVel{0:1} <custom_RN_value>
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
<custom_RN_value> is a double.
Query Syntax
:MEASure:JITTerN:NOISe:RNCValue:LEVel{0:1}?
Description
When using custom RN compensation (see :MEASure:JITTer:NOISe:RNComp), this command lets you specify the custom RN values for the symbol levels.