:MEASure:JITTer:NOISe:RNComp
Command Syntax
:MEASure:JITTerN:NOISe:RNComp {OFF | AUTomatic | CUSTom}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:NOISe:RNComp?
Description
This command disable disables RN compensation (OFF), enables compensation for oscilloscope RN (AUTomatic), or enables user-defined values for RN compensation (CUSTom).
If there are known contributors to random noise, you can use RN Compensation to compensate or remove noise from the measurement results.
When CUSTom is selected, use the :MEASure:JITTer:NOISe:RNCValue:LEVel command to specify the appropriate RN compensation values for the symbol levels.