:MEASure:JITTer:NOISe:RNSTabilize

Command Syntax

:MEASure:JITTerN:NOISe:RNSTabilize {ON | OFF | 1 | 0}

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Query Syntax

:MEASure:JITTerN:NOISe:RNSTabilize?

Query Response

{1 | 0}

Description

Enables or disables RN stabilization, which locks (stabilizes) the value of the measured RN that is used in amplitude measurements.

Use RN stabilization to prevent any uncorrelated non-Gaussian, non-periodic amplitude noise from falsely contributing to any measured RN value. One use of RN stabilization is to prevent cross talk, from an adjacent channel, appearing as noise.

When stabilization is on, the measurement pane shows an asterisk is shown next to the RN (rms) measurment results warning you that the measurement result has been modified. Above the table the annotation "*RN Fixed (1/0) at:" lists the entered values.

Use the :MEASure:JITTer:NOISe:RNSValue:LEVel command to specify the appropriate RN values for the symbol levels or use the   command to automatically use the current RN values.