:MEASure:LIST:ITEM{N}:COUNt?
Query Syntax
:MEASure:LIST:ITEM{N}:COUNt?
Where {N} is a number from 1 to 64 that identifies a measurement row in the Results table. For example, ITEM4.
Query Response
<value>
Description
For the measurement at the Results table row specified by ITEM{N}, returns the measurement's Count result value.
You can query the status of the Count result value using :MEASure:LIST:ITEM{N}:COUNt:STATus?.
If there is an invalid or questionable status, you can query for the reason using :MEASure:LIST:ITEM{N}:COUNt:STATus:REASon?.