:MEASure:LIST:ITEM{N}:MAXimum?

Query Syntax

:MEASure:LIST:ITEM{N}:MAXimum?

Where {N} is a number from 1 to 64 that identifies a measurement row in the Results table. For example, ITEM4.

Query Response

<value>

Description

For the measurement at the Results table row specified by ITEM{N}, returns the measurement's Maximum result value.

You can query the status of the Maximum result value using :MEASure:LIST:ITEM{N}:MAXimum:STATus?.

If there is an invalid or questionable status, you can query for the reason using :MEASure:LIST:ITEM{N}:MAXimum:STATus:REASon?.