:MEASure:LIST:SELect

Command Syntax

:MEASure:LIST:SELect  <index>

<index> is an int.

Query Syntax

:MEASure:LIST:SELect?

Description

In the Results table, selects a measurement in the active measurement list. Annotations for the selected measurement are placed on the displayed waveform at the level or coordinate used to calculate the final measurement result.

The argument is an index number that specifies the measurement to select. The active measurement list is indexed starting at 1. As a result, the first (top most) measurement in the list is identified as 1, the second measurement from the top is identified as 2, and so forth. To get the index value for a specific measurement, use the :LOCation? child command for the targeted measurement. For example, use :MEASure:HORizontal:FTIMe:LOCation?.

Example Command Sequence

Read the measurement location in the active measurement list, send the SELect command using the returned value. In this case 2.

:MEASure:HORizontal:FTIMe:LOCation?
…
…
:MEASure:LIST:SELect 2

Related Commands