:MEASure:LIST:ITEM{N}:STATus:REASon?
Query Syntax
:MEASure:LIST:ITEM{N}:STATus:REASon?
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
Returns a string that explains the reason for an invalid or questionable measurement selected by index ITEM{N} If the measurement was successful, a null string is returned.
Use the :MEASure:LIST:ITEM{N}:STATus? parent query to determine if the measurement results are invalid or questionable.
Additional information about an invalid or questionable measurement may be available using the :MEASure:LIST:ITEM{N}:STATus:DETails? sibling query.