:MEASure:LIST:ITEM{N}:SDEViation:STATus?

Query Syntax

:MEASure:LIST:ITEM{N}:SDEViation:STATus?

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid.
QUES
The measurement result is questionable.

Description

For the measurement specified by index ITEM{N} and its Std Dev results value returned by :MEASure:LIST:ITEM{N}:SDEViation?, this query returns the status of the Std Dev results value.

Use the :MEASure:LIST:ITEM{N}:SDEViation:STATus:REASon? child query to determine the reason for an invalid or questionable measurement.

See Also