:MEASure:LIST:ITEM{N}:STATus:DETails?
Query Syntax
:MEASure:LIST:ITEM{N}:STATus:DETails?
Description
Returns a string that may provide additional details for an invalid or questionable measurement selected by index ITEM{N}. If the measurement was successful, a null string is returned.
Use the :MEASure:LIST:ITEM{N}:STATus? parent query to determine if the measurement results are invalid or questionable.
For a basic description of an invalid or questionable measurement, use the :MEASure:LIST:ITEM{N}:STATus:REASon? sibling query.