:SYSTem:PERSona:MODel
Command Syntax
:SYSTem:PERSona:MODel "model number"
"model number" is a string.
Query Syntax
:SYSTem:PERSona:MODel?
Description
Specifies the model number of this product. If Infiniium is running on an oscilloscope, the default model number is something like "XR804KA". If Infiniium is running on a PC, the default model number is "D9300A".
Example Command Sequence
:SYSTem:PERSona:MODel "D9300A"