:SYSTem:TIME?

Query Syntax

:SYSTem:TIME?

Description

Queries the time in Infiniium in 24-hour format. The time is returned as a string with comma-separated values of <hour>,<minute>,<seconds>. For example,

"08,55,10"

which represents 8:55 am and 10 seconds. If the time was 8:55 pm instead, the time returned by the string would be:

"20,55,10"

Use the :SYSTem:DATE? query to return the date. Use the :SYSTem:UTCNow? query to return the Coordinated Universal Time (UTC).