:SYSTem:PERSona:MODel:DEFault
Command Syntax
:SYSTem:PERSona:MODel:DEFault
Query Syntax
:SYSTem:PERSona:MODel:DEFault?
Description
Sets the model identification string to its default value. If Infiniium is running on an oscilloscope, the default model number is something like "XR804KA". If Infiniium is running on a PC, the default model number is "D9300A".