:SYSTem:TEMPerature:STABle?

Query Syntax

:SYSTem:TEMPerature:STABle?

Query Response

{1 | 0}

Description

This query returns 0 if the oscilloscope's temperature is outside of the calibrated range or 1 if it is within the range.