:SYSTem:SERVice:MANagement:CALibration:INFormation?
Query Syntax
:SYSTem:SERVice:MANagement:CALibration:INFormation?
Description
This query returns the instrument calibration information in JSON format. The returned value includes the following:
- CalID – Calibration ID number created by the service center when the instrument was calibrated.
- CalBy – Service center that calibrated this instrument – either "Keysight Technologies" or "Keysight Authorized Calibration Provider".
- CalDate – Date of last calibration.
- CalDueDate – Calibration due date. The due date is calculated as CalDate + Calibration Interval, unless a shelf life policy is applied (see details).
- Status – returned value depends on:
- If SystemTime ≤ CalDueDate, Status is "CalibrationValid".
- If SystemTime > CalDueDate, Status is "CalibrationRequired".
- If CalDueDate is empty, and CalDate is presented, Status is "CalibrationValid".
- If SystemTime < CalDate, Status is "CalibrationUnknown".
- If Cal Data is unavailable, Status is "CalibrationNotFound".
- SystemTime – Current system time.
Example
:SYSTem:SERVice:MANagement:CALibration:INFormation?
'returns this format:
{"CalId":"1-00000000000-1","CalBy":"Keysight
Technonlogies","CalDate":"27-May-2020","CalDueDate":"27-
May-2021","Status":"CalibrationValid","SystemTime":"2020-
11-18 10:38:08"}