:SYSTem:SERVice:MANagement:CALibration:NOTification:ENABle
Command Syntax
:SYSTem:SERVice:MANagement:CALibration:NOTification:ENABle {{ON | 1} | {OFF | 0}}
Query Syntax
:SYSTem:SERVice:MANagement:CALibration:NOTification:ENABle?
Query Response
{1 | 0}
Description
This command sets and returns the calibration status/due popup notification state while the instrument is running. If disabled, the notification will pop up only on power up. If enabled, the notification will also pop up at 12:00 AM every day when the current date is ≤ the Cal Due Reminder days set by :SYSTem:SERVice:MANagement:CALibration:REMinder.
-
OFF— Popup notification is NOT visible while the instrument is running. -
ON— Popup notification is visible during instrument running.
Example
:SYSTem:SERVice:MANagement:CALibration:NOTification:ENABle OFF