:SYSTem:SERVice:MANagement:CALibration:PASScode[:VALue]
Command Syntax
:SYSTem:SERVice:MANagement:CALibration:PASScode[:VALue] <value>
<value> is a quoted string of the latest saved password. The default is: 'Key4Cal'
Description
This command lets you input the existing passcode and enable all setting features.
Example
:SYSTem:SERVice:MANagement:CALibration:PASScode:VALue '1q2w3e4r'