:SYSTem:SERVice:MANagement:CALibration:REMinder

Command Syntax

:SYSTem:SERVice:MANagement:CALibration:REMinder <value>

<value> is an integer value of 30, 15, or 7. The default is 30.

Query Syntax

:SYSTem:SERVice:MANagement:CALibration:REMinder?

Description

This command sets and returns the calibration due reminder days.

Example

:SYSTem:SERVice:MANagement:CALibration:REMinder 30