:SYSTem:SERVice:MANagement:CALibration:INTerval:VALue

Command Syntax

:SYSTem:SERVice:MANagement:CALibration:INTerval:VALue <value>

<value> is an integer between 1 and 120 that is the calibration interval in months.

Query Syntax

:SYSTem:SERVice:MANagement:CALibration:INTerval:VALue?

Query Response

<value>

Description

This command sets and returns the calibration interval value (interval in months).

Notes:

  • If using this command to set to the calibration interval, the calibration interval type (see :SYSTem:SERVice:MANagement:CALibration:INTerval:TYPE?) will be switched to user defined ("CUSTomer").
  • This command returns only the value of current saved calibration interval type. Any unsaved changes will not be returned.

Example

:SYSTem:SERVice:MANagement:CALibration:INTerval:VALue 12