:SYSTem:SERVice:MANagement:CALibration:PASScode

Command Syntax

:SYSTem:SERVice:MANagement:CALibration:PASScode <value>

<value> is a quoted string of the latest saved password. The default is: 'Key4Cal'

Description

This command lets you input the existing passcode and enable all setting features.

Example

:SYSTem:SERVice:MANagement:CALibration:PASScode '1q2w3e4r'