:SYSTem:SERVice:MANagement:CALibration:PERiodic:ENABle

Command Syntax

:SYSTem:SERVice:MANagement:CALibration:PERiodic:ENABle {{ON | 1} | {OFF | 0}}

Query Syntax

:SYSTem:SERVice:MANagement:CALibration:PERiodic:ENABle?

Query Response

{1 | 0}

Description

This command sets and returns the periodic calibration state:

  • OFF — Periodic calibration is disabled.

  • ON — Periodic calibration is enabled.

Example

:SYSTem:SERVice:MANagement:CALibration:PERiodic:ENABle ON