To better understanding how to use the E5072A, this section describes the basic measurement procedure using the E5072A and presents an example of the transmission measurement of a bandpass filter.
Basic Measurement Flow
Presetting the E5072A
Select:
S-parameter
Data format
Frequency range
Number of measurement points
Power level
IF bandwidth
Specify calibration kit
Select calibration type
Measure calibration data
Save calibartion data
Connect DUT
Adjust the scale
Analysis using markers
Store measurement file to a disk