File | Instrument | Response | Stimulus | Utility | Cal | Apps | Remote ONLY
Trace | Channel | Display-Window Setup | Display-Sheet Setup | Display Setup | External Devices | External Sources | PMAR | External DC Source | External Pulse Generators | New Measurement | Delete Measurement | Manage Meas | Balanced Meas |
Hardware: External Test Set
|
Description |
SCPI |
|
|---|---|---|
|
New Trace |
|
|
|
Select Trace |
|
|
|
Measure |
|
|
|
Trace Title |
|
|
|
Add Trace |
|
|
|
Delete Trace |
|
|
|
Move Trace |
|
|
|
Hold Trace |
|
|
|
Set/get the number of traces of selected channel |
|
|
|
Trace Maximize |
|
|
|
Add |
None |
|
Make Active |
None |
|
Read Channel Number |
|
|
Read UNUSED channel numbers |
None |
|
Read used channel numbers |
None |
|
Read number of Channels |
None |
|
Copy ONLY mechanical switches and attenuator settings. |
|
|
Delete a channel |
|
|
Set and return the group of channels |
|
|
Set and return the Multi DUT parallel measurement state |
|
|
Get the information if the parallel measurement is executed in the last sweep |
|
|
Set up multiple channels for manual trigger |
|
|
Select Window |
|
|
Window Title |
|
|
Add Window |
|
|
Delete Window |
|
|
Move Window |
|
|
Window Layout |
|
|
Window Max |
|
|
Return Window Number(s) |
|
|
Read the window number of the selected trace |
|
|
Creates N windows |
|
|
Feed specified measurement to specified window |
|
|
Returns the next unused trace number |
|
|
Set graph divisions |
|
|
Select Sheet |
|
|
Sheet Title |
|
|
Add Sheet |
|
|
Delete Sheet |
|
|
Sheet Layout |
|
|
Get list of window numbers which the sheet contains |
|
|
Feed specified window to a sheet |
|
|
Return active sheet number |
|
|
Return list of visible sheets |
|
|
Trace Status |
|
|
Y-axis Labels |
|
|
Show Marker Readout |
|
|
Large Readout |
|
|
Readouts Per Trace |
|
|
Sets the marker readouts to coupled (one combination annotation) or not coupled (one annotation per trace). |
|
|
Shows the marker readouts only for active trace or for all traces. |
|
|
Symbol - Triangle, Flag, and Line |
|
|
Decimal Places - Stimulus and Response |
|
|
Readout Position - X and Y |
|
|
Marker Colors |
|
|
N Trace: Markers |
|
|
N Trace: Memory Markers |
|
|
Reset Color |
|
|
Save Theme |
|
|
Recall Theme |
|
|
Reset Theme |
|
|
Grid Lines - Solid | Dotted |
|
|
Y-axis Divisions - 2 to 30 |
|
|
Show Table - None, Marker, Limit, Ripple, and Segment |
|
|
Toolbar Softkey |
|
|
Toolbar Hardkey |
|
|
Toolbar Port Extensions |
|
|
Toolbar Transform |
|
|
Toolbar Marker |
|
|
Toolbar Cal Set Viewer |
|
|
Active Entry Toolbar |
|
|
Toolbar Status Bar |
|
|
Status Bar |
|
|
Status Bar Clock |
|
|
Default Colors |
|
|
Background Colors |
|
|
Active Background Color |
|
|
Grid Colors |
|
|
Active Labels, Grid Frame Colors |
|
|
Inactive Window Labels Colors |
|
|
Failed Trace Colors |
|
|
N Trace: Data and Limits Colors |
|
|
N Trace: Memory |
|
|
Display Update |
|
|
Adds an external device to the system. |
|
|
Returns names of all configured devices |
|
|
Set driver for the external device. |
|
|
Set type of device. |
|
|
Configuration path for external device. |
|
|
Enable or disable communication with device. |
|
|
Sets and returns the name of the External Device. |
None |
|
Activation state of the device. |
|
|
Time out value for external device. |
|
|
Remove a device |
|
|
Save configuration file |
|
|
Load configuration file |
|
|
Returns if specified device responds |
|
|
Set Dwell per Point |
|
|
Set Trigger Mode |
|
|
Set Trigger Port |
|
|
Set Modulation Control |
|
|
Power Meter As Receiver (PMAR) Config See commands to configure and specify a Non- PMAR Power Sensor |
|
|
Enable use of internal cal factors |
|
|
Enable min and max freqs |
|
|
Set Max freq |
|
|
Set Min freq |
|
|
Set max number of PM readings |
|
|
Set tolerance level |
|
|
Select sensor |
|
|
Set Cal Factor data |
|
|
Set Cal Factor frequencies |
|
|
Set Power loss data |
|
|
Set Power loss frequencies |
|
|
Enable Power loss data |
|
|
Set reference cal factor |
|
|
Set Zero method |
|
|
Perform Cal |
|
|
|
||
|---|---|---|
|
Correction ON/OFF |
|
|
|
Offset correction value. |
|
|
|
Scale correction value. |
|
|
|
DC Type (Units). |
|
|
|
Dwell Before/After Point |
|
|
|
Dwell Before Sweep value |
|
|
|
Set and return the maximum output current value of the external DC Source |
|
|
|
Set and return the maximum output voltage value of the external DC Source |
|
|
|
Set and return the DC Meter/DC Source Abort Sweep command |
AbortSweepCmd |
|
|
Set and return the DC Meter/DC Source After Sweep command |
AfterSweepCmd |
|
|
Set and return the DC Meter/DC Source Before Sweep command |
BeforeSweepCmd |
|
|
Set and return the DC Meter/DC Source Error Query command |
ErrorQuery |
|
|
Set and return the DC Meter/DC Source Disable I/O command |
ExitCmd |
|
|
Set and return the DC Meter/DC Source ID Query command |
IDQuery |
|
|
Set and return the DC Meter/DC Source Enable I/O command |
InitCmd |
|
|
Set and return the DC Source maximum output |
MaxOutput |
|
|
Set and return the DC Source maximum output state |
MaxOutputState |
|
|
Set and return the DC Source minimum output |
MinOutput |
|
|
Set and return the DC Source minimum output state |
MinOutputState |
|
|
Set and return the Point Read commands and Point Set commands |
PointCmd |
|
|
||
|---|---|---|
|
PG Names catalog |
|
|
|
Read the integer of the name |
Not applicable |
|
|
Set output channel |
|
|
|
Set output Hi amplitude (volts) |
|
|
|
Set output Low amplitude (volts) |
|
|
|
Set load impedance |
|
|
|
Set source impedance |
|
|
|
Master Mode |
|
|
|
Optional Name/ID argument added to some Pulse gen commands. |
|
|
Create S-Parameter Meas. |
|
|
Create Measurement |
|
|
Add Measurement |
None |
|
List Measurements |
|
|
Delete a measurement |
|
|
Delete ALL measurements |
|
|
Get a handle to a Trace |
None |
|
Select a Measurement Parameter |
|
|
Read Channel Number |
|
|
Read Channel Numbers in use |
|
|
Read Number of Measurements |
None |
|
Read Measurement Parameter |
None |
|
Set / Read Measurement Name |
|
|
Read Active Measurement Number |
|
|
Change Parameter |
|
|
Returns the Measurement Class name |
|
|
Read the window number of the selected trace |
|
|
Read the trace number of the selected trace |
|
|
Maximize (Isolate) trace |
|
|
Move a trace to another window |
|
|
Trace Hold |
|
|
Trace Hold Clear |
|
|
Deletes the trace associated with the specified measurement number |
|
|
Create a new trace in the specified window |
|
|
Turn the memory trace ON or OFF for the specified measurement |
|
|
Move a trace associated with measurement number to the specified window |
|
|
Activate the specified measurement to be selected |
|
|
Turn trace display associated with the specified measurement ON or OFF |
|
|
Set or return the title for the specified measurement |
|
|
Turn the measurement title ON or OFF |
|
|
Autoscale the specified trace in the specified measurement |
|
|
Set the Y axis Scale Per Division value of the specified trace associated with the specified measurement |
|
|
Set the Y axis Reference Level of the specified trace associated with the specified measurement |
|
|
Set the Reference Position of the specified trace associated with the specified measurement |
|
|
|
|
|
Configure Topology |
|
|
Configure Balanced Measurement |
|
|
Maps the physical VNA ports to a device of balanced and single-ended logical ports for multi-port systems with greater than 4 ports |
|
|
Returns a list of currently supported test sets. |
|
|
Load config file and Restart VNA. |
|
|
Loads a test set configuration file. (and SCPI only - sets ID value). |
|
|
Returns the test set model |
|
|
Returns the test set ID number. |
None |
|
Returns the number of input ports |
|
|
Switches an input to one of the valid outputs (E5091A only). |
None |
|
Returns the total number of ports on the test set. |
|
|
Sets and returns the address for the external test set at the specified ID. |
|
|
Turns ON/OFF the port mapping and control line output. |
|
|
Sets and returns the port mappings for ALL ports. |
|
|
Sets and returns the mapping for a single port. |
|
|
Returns the label on a given channel. |
|
|
Turns ON/OFF status bar display of test set properties. |
|
|
Sets the control lines. |
|
|
Returns the selections available for a given logical port. |
|
|
Reads a Cal Set for the Test Set model. |
|
|
Reads a Cal Set for the Port Mapping. |
|
|
All Sense Multiplexer commands |
|
|
All Control Multiplexer commands (E5092A only) |
|