Last updated: October 19, 2012
The
Uplink Channel setting specifies the uplink UTRA Absolute
RF Channel Number (UARFCN). This automatically sets the test set's
receivers to the expected UE transmit frequency.
The relationship between UARFCN and uplink frequency is described in 3GPP TS 25.101 section 5.
| Band | TS 25.101 DL to UL Frequency Separation (MHz) |
TS 25.101 Center Frequency Range (MHz) |
TS 25.101 UARFCN Equation |
TS 25.101 UARFCN Range |
Test Set "Uplink Channel" Range |
|---|---|---|---|---|---|
| I (IMT-2000) |
190 | 1922.4 - 1977.6, increment = 0.2 |
5 * (center freq in MHz) | ||
| II (U.S. PCS) |
80 | 1852.4 - 1907.6, increment = 0.2 |
5 * (center freq in MHz) | 9262 - 9538 | 9262 - 9538 |
| 1852.5 - 1907.5, increment = 5 |
5 * ((center freq in MHz) - 1850.1 MHz) | 12, 37, 62, 87, 112, 137, 162, 187, 212, 237, 262, 287 | 12, 37, 62, 87, 112, 137, 162, 187, 212, 237, 262, 287 | ||
| III (DCS/PCS) |
95 | 1712.4 - 1782.6, increment = 0.2 |
5 * ((center freq in MHz) - 1525 MHz) | 937 - 1288 | 937 - 1288 |
| IV | 400 | 1712.4 - 1752.6, increment = 0.2 |
5 * ((center freq in MHz) - 1450 MHz) | 1312 - 1513 | 1312 - 1513 |
| 1712.5 - 1752.5, increment = 5 |
5 * ((center freq in MHz) - 1380.1 MHz) | 1662, 1687, 1712, 1737, 1762, 1787, 1812, 1837, 1862 | 1662, 1687, 1712, 1737, 1762, 1787, 1812, 1837, 1862 | ||
| V (US Cellular) |
45 | 826.4 - 846.6, increment = 0.2 |
5 * (center freq in MHz) | 4132 - 4233 | 4132 - 4233 |
| 826.5, 827.5, 831.5, 832.5, 837.5, 842.5 | 5* ((center freq in MHz) - 670.1 MHz) | 782, 787, 807, 812, 837, 862 | 782, 787, 807, 812, 837, 862 | ||
| VI (Japan 800) |
45 | 832.4 - 837.6, increment = 0.2 |
5 * (center freq in MHz) | 4162 - 4188 | 4162 - 4188 |
| 832.5, 837.5 | 5 * ((center freq in MHz) - 670.1 MHz) | 812, 837 | 812, 837 | ||
| VII | 120 | 2502.4 - 2567.6, increment = 0.2 |
5 * ((center freq in MHz) - 2100 MHz) | 2012 - 2338 | 2012 - 2338 |
| 2502.5 - 2567.5, increment = 5 |
5 * ((center freq in MHz) - 2030.1 MHz) | 2362, 2387, 2412, 2437, 2462, 2487, 2512, 2537, 2562, 2587, 2612, 2637, 2662, 2687 | 2362, 2387, 2412, 2437, 2462, 2487, 2512, 2537, 2562, 2587, 2612, 2637, 2662, 2687 | ||
| VIII | 45 | 882.4 - 912.6 | 5 * ((center freq in MHz) - 340 MHz) | 2712 - 2863 | 2712 - 2863 |
| IX | 95 | 1752.4 - 1782.4, increment = 0.2 |
5 * (center freq in MHz) | 8762 - 8912 | 8762 - 8912 |
| X | 400 | 1712.4 - 1767.6, increment = 0.2 |
5 * ((center freq in MHz) - 1135 MHz) | 2887 - 3163 | 2887 - 3163 |
| 1712.5-1767.5, increment = 5 |
5 * ((center freq in MHz) - 1075.1 MHz) | 3187, 3212, 3237, 3262, 3287, 3312, 3337, 3362, 3387, 3412, 3437, 3462 | 3187, 3212, 3237, 3262, 3287, 3312, 3337, 3362, 3387, 3412, 3437, 3462 | ||
| XI | 48 | 1430.4 - 1450.4, increment = 0.2 |
5 * ((center freq in MHz) - 733 MHz) | 3487 - 3562 | 3487 - 3562 |
| XII | 30 | 700.4 - 713.6, increment = 0.2 |
5 * ((center freq in MHz) + 22 MHz) | 3612 - 3678 | 3612 - 3678 |
| 700.5, 701.5, 706.5, 707.5, 712.5, 713.5 | 5 * ((center freq in MHz) + 39.9 MHz) | 3702, 3707, 3732, 3737, 3762, 3767 | 3702, 3707, 3732, 3737, 3762, 3767 | ||
| XIII | 31 | 779.4 - 784.6, increment = 0.2 |
5 * ((center freq in MHz) - 21 MHz) | 3792 - 3818 | |
| 779.5, 784.5 | 5 * ((center freq in MHz) - 11.1 MHz) | 3842, 3867 | 3842, 3867 | ||
| XIV | 30 | 790.4 - 795.6, increment = 0.2 |
5 * ((center freq in MHz) - 12 MHz) | 3892 - 3918 | 3892 - 3918 |
| 790.5, 795.5 | 5 * ((center freq in MHz) - 2.1 MHz) | 3942, 3967 | 3942, 3967 | ||
| 462 - 512 |
You can specify the uplink UARFCN in one of two ways:
Directly
set the Uplink Channel setting
to a specific uplink UARFCN value.
GPIB commands: CALL:UPLink:CHANnel[:MCHannel]
DL Channel Setting
When Uplink Channel is set to Auto , the uplink UARFCN is
automatically determined by the DL Channel
setting (the test set subtracts the frequency separation associated
with the DL Channel 's
band from the DL Channel setting).
GPIB command: CALL:UPLink:CHANnel:CONTrol:AUTO
To query the current uplink channel number via GPIB command, see CALL:STATus:UPLink:CHANnel? . Current Info, UL: Channel and Frequency is also displayed on the Channel (UARFCN) Information screen.
When in FDD Test operating mode, the expected
uplink frequency can also be set by manually entering the Uplink Frequency (see Receiver Control ).
Cell Off operating mode when changing these settings.
See CALL:OPERating
to select operating modes. Uplink
Channel setting is overwritten with the value of the
handover uplink channel . Uplink Channel setting results
in an UL/DL offset of less than 30 MHz when compared with
the DL
Channel setting, the warning message "Performance
not specified for UL/DL frequency offset <30 MHz"
is issued.Manual Operation: Setting Call Parameters that Can Only Be Changed in Cell Off Mode