Last updated: October 19, 2012
The
DL Channel
setting specifies the downlink UTRA Absolute RF Channel Number (UARFCN). This determines at what frequency the test set's RF generator will transmit the downlink signal.
The relationship between UARFCN and downlink frequency is described in 3GPP TS 25.101 section 5.
| Band |
TS 25.101 DL to UL Frequency Separation (MHz) |
TS 25.101 Center Frequency Range (MHz) |
TS 25.101 UARFCN Equation |
TS 25.101 UARFCN Range |
Test Set "DL Channel" Range |
|---|---|---|---|---|---|
|
I (IMT-2000) |
190 |
2112.4 - 2167.6, increment = 0.2 |
5 * (center freq in MHz) | ||
|
II (U.S. PCS) |
80 |
1932.4 - 1987.6, increment = 0.2 |
5 * (center freq in MHz) | 9662 - 9938 | 9662 - 9938 |
|
1932.5 - 1987.5, increment = 5 |
5 * ((center freq in MHz) - 1850.1 MHz) | 412, 437, 462, 487, 512, 537, 562, 587, 612, 637, 662, 687 | 412, 437, 462, 487, 512, 537, 562, 587, 612, 637, 662, 687 | ||
|
III (DCS/PCS) |
95 |
1807.4 - 1877.6, increment = 0.2 |
5 * ((center freq in MHz) - 1575 MHz) | 1162 - 1513 | 1162 - 1513 |
| IV | 400 |
2112.4 - 2152.6, increment = 0.2 |
5 * ((center freq in MHz) - 1805 MHz) | 1537 - 1738 | 1537 - 1738 * |
|
2112.5 - 2152.5, increment = 5 |
5 * ((center freq in MHz) - 1735.1 MHz) | 1887, 1912, 1937, 1962, 1987, 2012, 2037, 2062, 2087 | 1887, 1912, 1937, 1962, 1987, 2012, 2037, 2062, 2087 * | ||
|
V (US Cellular) |
45 |
871.4 - 891.6, increment = 0.2 |
5 * (center freq in MHz) | 4357 - 4458 | 4357 - 4458 # |
| 871.5, 872.5, 876.5, 877.5, 882.5, 887.5 | 5* ((center freq in MHz) - 670.1 MHz) | 1007, 1012, 1032, 1037, 1062, 1087 | 1007, 1012, 1032, 1037, 1062, 1087 # | ||
|
VI (Japan 800) |
45 |
877.4 - 882.6, increment = 0.2 |
5 * (center freq in MHz) | 4387 - 4413 | 4387 - 4413 + |
| 877.5, 882.5 | 5 * ((center freq in MHz) - 670.1 MHz) | 1037, 1062 | 1037, 1062 + | ||
| VII | 120 |
2622.4 - 2687.6, increment = 0.2 |
5 * ((center freq in MHz) - 2175 MHz) | 2237 - 2563 | 2237 - 2563 |
|
2622.5 - 2687.5, increment = 5 |
5 * ((center freq in MHz) - 2105.1 MHz) | 2587, 2612, 2637, 2662, 2687, 2712, 2737, 2762, 2787, 2812, 2837, 2862, 2887, 2912 | 2587, 2612, 2637, 2662, 2687, 2712, 2737, 2762, 2787, 2812, 2837, 2862, 2887, 2912 | ||
| VIII | 45 |
927.4 - 957.6, increment = 0.2 |
5 * ((center freq in MHz) - 340 MHz) | 2937 - 3088 | 2937 - 3088 |
| IX | 95 |
1847.4 - 1877.4, increment = 0.2 |
5 * (center freq in MHz) | 9237 - 9387 | 9237 - 9387 * |
| X | 400 |
2112.4 - 2167.6, increment = 0.2 |
5 * ((center freq in MHz) - 1490 MHz) | 3112 - 3388 | 3112 - 3388 * |
|
2112.5 - 2167.5, increment = 5 |
5 * ((center freq in MHz) - 1430.1 MHz) | 3412, 3437, 3462, 3487, 3512, 3537, 3562, 3587, 3612, 3637, 3662, 3687 | 3412, 3437, 3462, 3487, 3512, 3537, 3562, 3587, 3612, 3637, 3662, 3687 * | ||
| 5 * ((center freq in MHz) - 736 MHz) | |||||
| 5 * ((center freq in MHz) + 37 MHz) | |||||
| 730.5, 731.5, 736.5, 737.5, 742.5, 743.5 | 5 * ((center freq in MHz) + 54.9 MHz) | 3927, 3932, 3957, 3962, 3987, 3992 | 3927, 3932, 3957, 3962, 3987, 3992 | ||
| 5 * ((center freq in MHz) + 55 MHz) | |||||
| 748.5, 753.5 | 5 * ((center freq in MHz) + 64.9 MHz) | 4067, 4092 | 4067, 4092 | ||
| 5 * ((center freq in MHz) + 63 MHz) | |||||
| 760.5, 765.5 | 5 * ((center freq in MHz) + 72.9 MHz) | 4167, 4192 | 4167, 4192 | ||
|
877.4- 887.6 |
712 to 763 | ||||
| 862 to 912 | |||||
|
#
In order to ensure a Frequency Band Indicator of Band V is sent in SIB5 when
+
In order to ensure a Frequency Band Indicator of Band VI is sent in SIB5 when * Ensure that the Transmit SIB5bis parameter is set accordingly for your UE. |
|||||
When in
FDD Test
operating mode, the downlink frequency can also be set by setting
RF Gen Freq Ctrl
to
Manual
and then manually entering the
RF Gen Freq
.
To set the downlink channel number via GPIB command, see CALL:CHANnel .
Cell Off
operating mode when changing this setting. See
CALL:OPERating
to select operating modes.
DL Channel
setting is overwritten with the value of the handover downlink channel
.
DL Channel
setting results in an UL/DL offset of less than 30 MHz when compared with the
Uplink Channel
setting, the warning message "Performance not specified for UL/DL frequency offset <30 MHz" is issued.