Last updated: January 15, 2009
Before performing these procedures, ensure that you have specified the proper Amplitude Offset for your test setup, and that the test set has been properly calibrated (see Calibrating the Test Set ).
RB Test Mode
connection between the UE and test set (see
How Do I Set Up a Call and Make a Connection?
).
Active Bits
(this is the default setting).
21 dBm
).
Phase Discontinuity
measurement.
Phase Discont. Setup
(
F1
)
Graph Control
(
F2
).
Axis Control
(
F1
) to set the axis control parameters as needed:
Start
(
F1
) determines the first slot result displayed.
Span
(
F2
) determines the number of timeslots for which results are displayed.
Phase Reference
(
F3
on
Axis Control 1 of 2
).
Phase Range
(
F4
on
Axis Control 1 of 2
).
Power Ref
(
F3
on
Axis Control 2 of 2
).
Power Range
(
F4
on
Axis Control 2 of 2
).
Trace Show/Hide
(
F4
) to choose which of the 3 available traces to display (
Phase Discontinuity
,
Phase
and
Power
). Select
Close Menu
(
F6
).
Marker
(
F2
) to turn on the marker on the graphical display and move the highlighted bar in the numerical results display area. Scroll through the numerical data and locate the orange values indicating worst case phase discontinuity and worst case EVM to determine whether the UE has met specifications for this portion of the test.
Select
Table
(
F3
) to scroll through the 9 columns of numerical results available, as needed.
A typical result is pictured below:
Return
(
F6
).
Repeat steps 7-12 until the UE reaches its minimum output power (for example, -49 dBm). You can easily determine the UE's output power level by noting the
UE Target Power
level (
F7
on the
Call Parms 3 of 3
menu), because at the completion of the measurement, the test set sets
MS Target Power
to the UE's output power in the final measured slot).
You may choose to overlap the test subsequences by starting at an
MS Target Power
that is offset from the ending power level, see
Key 3GPP Tests Performed Using the Phase Discontinuity Measurement
for more information.
Phase Discont. Setup
(
F1
)
This section is applicable to the lab application or feature-licensed test application only.
This test is applicable to Release 6 and later HSDPA UEs. For Release 5 HSDPA UEs, see Measuring 3GPP TS 34.121 v7.5.0 s5.13.1A Error Vector Magnitude (EVM) with HS-DPCCH .
3GPP TS 34.121 5.13.1AA measures EVM and phase discontinuity at four locations on a defined 12 ms UE power pattern:
The test is performed such that the 12 ms UE power pattern maximum corresponds to the UE's maximum output power as defined in 34.121 Table 5.2A.2. The test is also performed such that the 12 ms UE power pattern maximum corresponds to -18 dBm.
Operating Mode
(
F1
) to
Cell Off
.
34.121 Preset Call Configurations
(
F11
on
Call Parms 1 of 3
) and select
5.2C, 5.7A, 5.13.1A, 5.13.1AA, 5.13.2A with QPSK
. You may then skip any steps marked with
[34.121 Call Config]
in this procedure.
Channel (UARFCN) Parms
(
F12
on
Call Parms 1 of 3
). Set
DL Channel
(
F7
) and
Uplink Channel
(
F8
) to the appropriate "low range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band II, set
DL Channel
=
9663
).
Uplink Parameters
(
F4
on
Call Control 2 of 5
).
Uplink DPCH Bc/Bd Control
to
Manual
.
Manual Uplink DPCH Bc
to
15
(for 34.121 v7.2.0 Table C.10.1.4 sub-test 3).
Manual Uplink DPCH Bd
to
8
(for 34.121 v7.2.0 Table C.10.1.4 sub-test 3).
Maximum Uplink Transmit Power Level
to
+21 dBm
.
Operating Mode
to
Active Cell
(pressing the
CALL SETUP
key quickly brings you back to the top level
Call Control
menu).
Channel Type
(
F8
) to
12.2k RMC + HSDPA
.
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
HSDPA RB Test Mode Setup
(
F8
).
HS-DSCH Configuration Type
to
FRC
(this is the default value).
FRC Type
to
H-Set 1 QPSK
(this is the default value).
CN Domain
as needed (by default it is set to
PS Domain
). Note, before you can establish a connection in the PS domain, the UE must attach to the test set. To enable this, the
PS Domain Information
parameter (under
Cell Parameters
,
F12
on
Call Control 2 of 5
) must be set to
Present
when the UE registers (attaches) with the test set.
HSDPA Uplink Parameters
(
F11
).
DeltaACK
and
DeltaNACK
to
8
.
DeltaCQI
to
7
.
Ack-Nack Repetition Factor
to
1
(this is the default value).
CQI Feedback Cycle (k)
to
4 ms
.
CQI Repetition Factor
to
1
(this is the default value).
Cell Parameters
(
F2
).
Cell Info (
F2
)
, then
Cell Parameters
(
F2
).
Call Control 2 of 5
menu)
Default DPCH Offset (DOFF)
to
3 x 512 chips
.
PS Domain Information
to
Present
(this is the default value in the lab application) if you plan to establish the HSDPA connection in the PS domain (i.e. if you've set
CN Domain
to
PS Domain
or
CS/PS Domain
in step 3 above).
Cell Info
,
Reselection Parameters
(
F3
).
Generator Info
(
F3
on
Call Control 2 of 5
), select
Connected DL Channel Levels
(
F4
), then select
HSDPA Conn DL Channel Levels
(
F4
).
Cell 1 Connected HSDPA CPICH Level
to
-10 dB
(this is the default value).
Cell 1 Connected HSDPA P-CCPCH/SCH Level
to
-12 dB
(this is the default value).
Cell 1 Connected HSDPA PICH Level
to
-15 dB
(this is the default value).
Cell 1 Connected HSDPA DPCH Level
to
-9 dB
.
Cell 1 Sum of Active Conn HS-PDSCH Levels
to
-3 dB
(this is the default value).
Cell 1 Connected HS-SCCH 1 Level
to
-8 dB
.
Originate Call
(
F3
on
Call Control 1 of 5
).
Cell Power
(
F7
on
Call Parms 1 of 3
) to
-86 dBm/3.84 MHz
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
).
To perform the test such that the 12 ms UE power pattern maximum corresponds to the UE's maximum output power as defined in 34.121 Table 5.2A.1, set
UE Target Power
(
F7
on
Call Parms 3 of 3
) to the appropriate value for your UE's power class.
| UE Power Class | 34.121 v7.5.0 Table C.10.1.4 Sub-Test | UE Target Power setting |
|---|---|---|
| 3 | 3 | 16.9 dBm |
| 4 | 3 | 13.9 dBm |
For example, for a power class 3 UE, set
UE Target Power
to
16.9 dBm
(the test set rounds this value to 17 dBm). The test set drives the UE's DPCCH+DPDCH level to 17 dBm, which places the UE's DPCCH+DPDCH+HS-DPCCH level at 23.1 dBm, while also appropriately ranging the test set's measurement receiver.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Alternating bits
.
Phase Discontinuity
.
Phase Discont Setup
(
F1
).
Trigger Source
to
HS-DPCCH
.
HS-DPCCH Trigger Subframe Alignment
to
subframe 0
(this is the default value).
HS-DPCCH Trigger Slot Alignment
to
AckNack (this is the default value)
.
HS-DPCCH Trigger Subslot Alignment
to
0.0 slot (this is the default value)
.
0.5 slot (this is the default value)
.
HS-DPCCH Measurement Step Count
to
21 (this is the default value)
.
Close Menu
(
F6
).
Graph Control
(
F2
) and adjust
Axis Control
(
F1
) as needed. Note that the
Power Ref
and
Power Range
can be adjusted by pressing the
More
(
1 of 2
) key. Select
Return
(
F6
).
Trace Show/Hide
(
F4
) to hide the
Phase
trace.
Marker
(
F2
) to verify that the measured EVM is less than 17.5% for test points 1, 2, 3 and 4 (marker indices 0, 1, 20 and 21), and that the phase discontinuity across points A and B (marker indices 1 and 21) is less than 36 degrees.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Active bits
.
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
-24.1 dBm
(for 34.121 v7.2.0 Table C.10.1.4 sub-test 3). The test set drives the UE's DPCCH+DPDCH level to -24 dBm, which places the UE's DPCCH+DPDCH+HS-DPCCH level at approximately -18 dBm, while also appropriately ranging the test set's measurement receiver.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Alternating bits
.Phase Discontinuity Measurement Description
Phase Discontinuity Troubleshooting
Programming the Phase Discontinuity Measurement
Measuring 3GPP TS 34.121 v7.5.0 s5.13.1A Error Vector Magnitude (EVM) with HS-DPCCH (using the Waveform Quality measurement)