Before performing these procedures, ensure that you have specified the proper Amplitude Offset for your test setup, and that the test set has been properly calibrated (see Calibrating the Test Set ).
Operating Mode
(
F1
) to
Cell Off
.
DL Channel
(
F10
) and
Uplink Channel
(
F11
) to the appropriate "low range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band I,
DL Channel
=
10563
and
Uplink Channel
=
9613
).
Operating Mode
to
Active Cell
.
RB Test Mode
connection between the UE and test set (see
How Do I Set Up a Call and Make a Connection?
).
Connected DL Channel Levels
are set to their default values, as required by 3GPP TS 34.121 Tables 5.3 and E.3.1 (select
Generator Info
,
F3
on
Call Control 2 of 5
).
Cell Power
(
F7
) to
-106.7 dBm
.
UE Target Power
:
UL CL Power Ctrl Mode
is set to its default value of
Active Bits
(select
UL CL Power Ctrl Parameters
,
F8
on the
Call Parms 3 of 3
menu).
UE Target Power
(
F7
) to the specified maximum output power for your UE (for example, 21 dBm for power class 4).The test set then drives the UE to the specified level, while also appropriately ranging its measurement receiver.
UL CL Power Ctrl Parameters
menu (
F8
) and set
UL CL Power Ctrl Mode
to
All Up bits
and ensure that
UL CL Power Ctrl Algorithm
is set to
Two
. The test set then drives the UE to transmit at the highest level possible.
Waveform Quality
.
Waveform Quality Setup
(F1) and set
Trigger Arm
to
Single
.
Frequency Error
is less than +/- (0.1 ppm + 10 Hz). For an uplink frequency of 1922.6 MHz, this corresponds to a frequency error requirement of +/- 202.26 Hz.
This section is applicable to the lab application or feature-licensed test application only.
This test is applicable to Release 5 UEs only. For Release 6 and later UEs, see Measuring 3GPP TS 34.121 v7.5.0 5.13.1AA Error Vector Magnitude (EVM) and Phase Discontinuity with HS-DPCCH .
3GPP TS 34.121 5.13.1A measures EVM at four locations on a defined 12 ms UE power pattern:
The test is performed such that the 12 ms UE power pattern maximum corresponds to the UE's maximum output power as defined in 34.121 Table 5.2A.2. The test is also performed such that the 12 ms UE power pattern maximum corresponds to -18 dBm.
Operating Mode
(
F1
) to
Cell Off
.
34.121 Preset Call Configurations
(
F11
on
Call Parms 1 of 3
) and select
5.2C, 5.7A, 5.13.1A, 5.13.1AA, 5.13.2A with QPSK
. You may then skip any steps marked with
[34.121 Call Config]
in this procedure.
Channel (UARFCN) Parms
(
F12
on
Call Parms 1 of 3
). Set
DL Channel
(
F7
) and
Uplink Channel
(
F8
) to the appropriate "low range" frequencies for your UE's operating band, as specified by 3GPP TS 34.108 5.1.1 (for example, for operating band II, set
DL Channel
=
9663
).
Uplink Parameters
(
F4
on
Call Control 2 of 5
).
Uplink DPCH Bc/Bd Control
to
Manual
.
Manual Uplink DPCH Bc
to
15
(for 34.121 v7.2.0 Table C.10.1.4 sub-test 3).
Manual Uplink DPCH Bd
to
8
(for 34.121 v7.2.0 Table C.10.1.4 sub-test 3).
Maximum Uplink Transmit Power Level
to
+21 dBm
.
Operating Mode
to
Active Cell
(pressing the
CALL SETUP
key quickly brings you back to the top level
Call Control
menu).
Channel Type
(
F8
) to
12.2k RMC + HSDPA
.
HSDPA Parameters
(
HSPA Parameters
(
F10
),
F10
).
HSDPA RB Test Mode Setup
(
F8
).
HS-DSCH Configuration Type
to
FRC
(this is the default value).
FRC Type
to
H-Set 1 QPSK
(this is the default value).
CN Domain
as needed (by default it is set to
PS Domain
). Note, before you can establish a connection in the PS domain, the UE must attach to the test set. To enable this, the
PS Domain Information
parameter (under
Cell Parameters
,
F12
on
Call Control 2 of 5
) must be set to
Present
when the UE registers (attaches) with the test set.
HSDPA Uplink Parameters
(
F11
).
DeltaACK
and
DeltaNACK
to
8
.
DeltaCQI
to
7
.
Ack-Nack Repetition Factor
to
1
(this is the default value).
CQI Feedback Cycle (k)
to
4 ms
.
CQI Repetition Factor
to
1
(this is the default value).
Cell Parameters
(
F2
).
Cell Info (
F2
)
, then
Cell Parameters
(
F2
).
Call Control 2 of 5
menu)
Default DPCH Offset (DOFF)
to
3 x 512 chips
.
PS Domain Information
to
Present
(this is the default value in the lab application) if you plan to establish the HSDPA connection in the PS domain (i.e. if you've set
CN Domain
to
PS Domain
or
CS/PS Domain
in step 3 above).
Cell Info
,
Reselection Parameters
(
F3
).
Generator Info
(
F3
on
Call Control 2 of 5
), select
Connected DL Channel Levels
(
F4
), then select
HSDPA Conn DL Channel Levels
(
F4
).
Cell 1 Connected HSDPA CPICH Level
to
-10 dB
(this is the default value).
Cell 1 Connected HSDPA P-CCPCH/SCH Level
to
-12 dB
(this is the default value).
Cell 1 Connected HSDPA PICH Level
to
-15 dB
(this is the default value).
Cell 1 Connected HSDPA DPCH Level
to
-9 dB
.
Cell 1 Sum of Active Conn HS-PDSCH Levels
to
-3 dB
(this is the default value).
Cell 1 Connected HS-SCCH 1 Level
to
-8 dB
.
Originate Call
(
F3
on
Call Control 1 of 5
).
Cell Power
(
F7
on
Call Parms 1 of 3
) to
-86 dBm/3.84 MHz
.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
).
To perform the test such that the 12 ms UE power pattern maximum corresponds to the UE's maximum output power as defined in 34.121 Table 5.2A.1, set
UE Target Power
(
F7
on
Call Parms 3 of 3
) to the appropriate value for your UE's power class.
| UE Power Class | 34.121 v7.5.0 Table C.10.1.4 Sub-Test | UE Target Power setting |
|---|---|---|
| 3 | 3 | 16.9 dBm |
| 4 | 3 | 13.9 dBm |
For example, for a power class 3 UE, set
UE Target Power
to
16.9 dBm
(the test set rounds this value to 17 dBm). The test set drives the UE's DPCCH+DPDCH level to 17 dBm, which places the UE's DPCCH+DPDCH+HS-DPCCH level at 23.1 dBm, while also appropriately ranging the test set's measurement receiver.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Alternating bits
.
You can you use the
Dynamic Power Analysis
measurement to quickly verify that your UE is transmitting the 12 ms power pattern specified by 5.13.1A. To do so, press the
Measurement selection
key and select
Dynamic Power Analysis
, then select
Dynamic Power Setup
(
F1
) and select
34.121 5.7A Measurement Configuration
, then
Yes
(or set
Steps
to
37
,
Step Length
to
333.3 us
,
Measurement Interval
to
283.3 us
,
Trigger Source
to
HS-DPCCH
,
Trigger Delay
to
-308.3 us
, and
HS-DPCCH Trigger Subframe Alignment
to
subframe 0
). Press
START SINGLE
and adjust the
Axis Control
(
F2
) as needed.
Once you have verified that your UE is transmitting the proper pattern, you can initiate the Waveform Quality measurement and adjust the Waveform Quality trigger settings to measure each test point:
Waveform Quality
.
Waveform Quality Setup
(
F1
).
34.121 5.13.1A Low of Low-High Transition
, then select
Yes
. You may then skip any steps marked with
[34.121 Meas Config]
.
Trigger Source
to
HS-DPCCH
.
Transient Period
to
Exclude
.
0.5 slot
.
Trigger Arm
to
Single
, if desired.
Close Menu
(
F6
).
Trigger Arm
to
Single
, press the
START SINGLE
key to begin the measurement.
Verify that the measured EVM is less than 17.5% for each of the four test points, using the following settings:
| These settings are automatically set by the 34.121 Meas Configs | ||||
|---|---|---|---|---|
| HS-DPCCH Trigger Subframe Alignment | HS-DPCCH Trigger Slot Alignment | HS-DPCCH Trigger Subslot Alignment | ||
| 1 | subframe 5 | CQI2 | 0.5 slot | |
| 2 | subframe 0 | AckNack | 0.0 slot | |
| 3 | subframe 3 | AckNack | 0.5 slot | |
| 4 | subframe 3 | CQI1 | 0.0 slot | |
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Active bits
.
UE Target Power
(
F7
on
Call Parms 3 of 3
) to
-24.1 dBm
(for 34.121 v7.2.0 Table C.10.1.4 sub-test 3). The test set drives the UE's DPCCH+DPDCH level to -24 dBm, which places the UE's DPCCH+DPDCH+HS-DPCCH level at approximately -18 dBm, while also appropriately ranging the test set's measurement receiver.
UL CL Power Ctrl Parameters
(
F8
on
Call Parms 3 of 3
). Set
UL CL Power Ctrl Mode
to
Alternating bits
.Waveform Quality Measurement Description
Waveform Quality Troubleshooting
Programming a Waveform Quality Measurement
How Do I Make a Dynamic Power Analysis Measurement?
Measuring 3GPP TS 34.121 v7.5.0 5.13.1AA Error Vector Magnitude (EVM) and Phase Discontinuity with HS-DPCCH (using the Phase Discontinuity measurement)