Last updated: January 16, 2009
This section provides an example of how to make phase discontinuity measurements via GPIB.
The basic procedure to perform phase discontinuity measurements is as follows:
 Active Bits 
(
CALL[:CELL]:CLPControl:UPLink:MODE
).10 ! Phase Discontinuity Measurement Programming Example 20 ! This programming example assumes that there is an RB 30 ! Test Mode connection between the test set and UE. 40 ! 50 Testset=714 60 ! 70 ! *** Set Up Test Parameters *** 80 ! 90 OUTPUT Testset;"CALL:CLPControl:UPLink:MODE ACTive" 100 ! Set UL CL Power Ctrl Mode to Active Bits. 110 OUTPUT Testset;"CALL:MS:POWer:TARGet 21" 120 ! Set MS Target Power to +21 dBm. 130 ! 140 ! *** Set Up Measurement Parameters *** 150 ! 160 OUTPUT Testset;"SETup:WPDiscon:PCPattern DN5_4UP" 170 ! Set Power Control Pattern to 5DOWN/4UP. 180 OUTPUT Testset;"SETup:WPDiscon:NPRepetition 10" 190 ! Set the Number of Pattern Repetitions to 10. 200 ! 210 ! *** INITiate and FETCh Measurements *** 220 ! 230 OUTPUT Testset;"INITiate:WPDiscon" 240 ! Initiate a Phase Discontinuity measurement. 250 OUTPUT Testset;"FETCh:WPDiscon?" 260 ! Fetch Phase Discontinuity measurement results. 270 ENTER Testset;Int,Num_slts,Wc_pd_slt,Wc_pd,Wc_evm_slt,Wc_evm 280 ! Retrieve the results. 290 ! 300 ! *** Print Measurement Results *** 310 ! 320 CLEAR SCREEN 330 PRINT "Phase Discontinuity Measurement Results:" 340 PRINT 350 PRINT "Integrity Indicator = ",Int 360 PRINT "Number of Slots Measured = ",Num_slts 370 PRINT "Worst Case Phase Discontinuity Slot Number = ",Wc_pd_slt 380 PRINT "Worst Case Phase Discontinuity (in degrees) = ",Wc_pd 390 PRINT "Worst Case EVM Slot Number = ",Wc_evm_slt 400 PRINT "Worst Case EVM (in % rms) = ",Wc_evm 410 ! 420 END
Phase Discontinuity Troubleshooting
Phase Discontinuity Measurement Description
Manual Operation: How Do I Make a Phase Discontinuity Measurement?