This section is only applicable to the lab application.
Operating Mode
(
F1
) to
Cell Off
.
DPCH 30 ksps (OVSF 128) Channelization Code
to 20, 29, 37, 45, 60, 70, 76, 87 or 93. For 64k downlink channels or the 57.6k UL/57.6k DL CS Data RAB you must set
DPCH 120 ksps (OVSF 32) Channelization Code
to 24-27. For all other supported channel types, the default DPCH channelization codes are valid. See
Channel Types Supported in Compressed Mode and Channelization Code Range
and
How Do I Change Generator Information?
.
DL Channel
,
RLC Reestablish
, etc. See
How Do I Set Up a Call and Make a Connection?
.
Operating Mode
(
F1
) to
Active Cell
.
Compressed Mode Info
(
F4
on
Call Control 4 of 5
).
Compressed Mode Parameters
(
F2
).
Shared Comp Mode Parms
(
F1
) as desired.
First
through
Fourth
TGPSs as desired (or use one of the
Compressed Mode Preset Configs
(
F5
) from the main compressed mode menu to quickly configure the TGPSs to one of six pre-defined configurations).
<num> TGPS State
and
<num> TG Measurement Purpose (TGMP)
accordingly for each TGPS.
UE Meas Setup
(
F3
).
UE Measurements in Compressed Mode
to
On
(so that the UE will report measurement results).
Measurement Configuration
to
InterfrequencyMeas
or
InterRATMeas
, depending upon whether you want the UE to measure W-CDMA (inter-frequency) or GSM neighbor cells, respectively. The UE may perform measurements on either GSM or W-CDMA neighbor cells when you enable compressed mode, but not both. Ensure that you have a TGPS active with a
TG Measurement Purpose
that matches the
Measurement Configuration
setting.
GSM Meas BSIC Verification
to
verifiedBSIC
, your UE will likely return empty Measurement Reports. If your UE supports BSIC verification you may still receive empty Measurement Reports when
GSM BSIC Verification
is set to
verifiedBSIC
if you do not include an active TGPS with a TGMP of
GSM Initial BSIC ID
or
GSM BSIC Reconfirmation
.
Compressed Mode Info
menu (
F4
on
Call Control 4 of 5
).
Enable Compressed Mode
(
F1
).
Overall CM
state changes to
On
, that the TGPSs you've specified are active, and no errors are posted (which would indicate that you've specified an invalid TGPS configuration that causes more than one transmission gap to occur in a single frame).
If you enabled UE measurements in step
B. Configure Compressed Mode and UE Measurements Setup Parameters
, then you can view the UE measurement results for either GSM or FDD (W-CDMA) neighbor cells (depending upon whether you set
Measurement Configuration
to
InterRATMeas
or
InterfrequencyMeas
). To change which type of cells are being measured and reported by the UE, you must disable compressed mode, change the Measurement Configuration setting, then enable compressed mode.
Compressed Mode Meas Results
(
F5
), then
GSM Measurement Results
(
F1
). Note that the cells are reported in order of RSSI strength rather than by cell ID. The cell ID for each cell (numbered 1 to 8) is returned to help you quickly determine which neighbor cell is being reported by the UE.
Compressed Mode Meas Results
(
F5
), then
FDD Inter-freq Meas Results (1 of 2)
(
F2
) or
FDD Inter-freq Meas Results (2 of 2)
(
F3
).
At this point, you may choose to perform receiver or transmitter testing on the UE, or perform call processing operations such as handovers. See Additional Considerations While in Compressed Mode Operation for information on the availability of these features while in compressed mode.