:CALibrate:CHANnel:ENABled
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CALibrate:CHANnel{1:8}{A|B|C|D}:ENABled {ENABled | DISabled}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CALibrate:CHANnelN:ENABled?
Description
Enables or disables a vertical calibration for the indicated module's input channel.
- ENABled
-
Selects all calibrations for the indicated slot to be performed. - DISabled
-
Prevents all calibrations for the indicated slot from being performed.
Use the child queries listed in the following table to return details about the current calibration.
| Status String | Child Query to Send |
|---|---|
| Time of last calibration, Time change since last calibration, and Temperature change since last calibration |
:DETails?
|
| Change in temperature | :DTEMperature?
|
| Change in Time | :TIME?
|
Requires FlexDCA revision A.02.00 and above.
Query Response
{ENAB | DIS}
- ENAB
-
Indicates that all calibrations for the indicated slot are selected. - DIS
-
Indicates that all calibrations for the indicated slot are disabled.
Example Command
:CALibrate:CHANnel2A:ENABled ENABled