:CALibrate:PROBe:CHANnel:STATus:DTEMperature?
Query Syntax
:CALibrate:PROBe:CHANnel{1:8}{A|B|C|D}:STATus:DTEMperature?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Queries the change in the N1000A frame's temperature from the time when the last frame calibration was performed. If a calibration has not yet been performed, a value of NaA (9.91E+37) is returned. A calibration should be performed if the change in N1000A temperature exceeds ±5°C.
Requires FlexDCA revision A.02.00 and above.
Example Returned Status
-6.10
Example Query
:CALibrate:PROBe:CHANnel2B:STATus:DTEMperature?