:CALibrate:PROBe:CHANnel:STARt
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CALibrate:PROBe:CHANnel{1:8}{A|B|C|D}:STARt
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Starts a calibration for a probe on the indicated channel. The *OPC? query should be used to detect when a portion of the calibration has completed. Use the :CALibrate:CONTinue command to dismiss dialogs that are displayed during a calibration.
Requires FlexDCA revision A.02.00 and above.
Example Command Sequence
:CALibrate:PROBe:CHAN3A:STARt *OPC? … // Your code to synchronize execution timing. :CALibrate:CONTinue *OPC? … // Your code to synchronize execution timing. :CALibrate:CONTinue