:CHANnel Subsystem

Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT

The Channel subsystem commands control all vertical (Y axis) functions. To control differential waveforms, use the :DIFF subsystem.

The commands in the :CHANnel subsystem, require a channel identifier which identifies the channel to which the command applies. The channel identifier includes the FlexDCA module slot number {1:8} followed by the module's channel letter {A|B|C|D}. For example, you can display channel 1A with any of the following four identical commands. (Notice channel identifier highlighted in red.)

:CHAN1A:DISPlay ON;
:CHANnel1A:DISPlay ON;

The following table shows the different possible forms of the :CHANnel SCPI subsystem node with the required channel specifier.

Varieties of the Channel Command (shown for slots 1 through 4 only)
Channel Command
Varieties
Channel Command>
Varieties
Channel Command
Varieties
Channel Command
Varieties
1A :CHANnel1A
:CHANnel11
2A :CHANnel2A
:CHANnel21
3A :CHANnel3A
:CHANnel31
4A :CHANnel4A
:CHANnel41
1B :CHANnel1B 2B :CHANnel2B 3B :CHANnel3B 4B :CHANnel4B
1C :CHANnel1C 2C :CHANnel2C 3C :CHANnel3C 4C :CHANnel4C
1D :CHANnel1D 2D :CHANnel2D 3D :CHANnel3D 4D :CHANnel4D

This form of the command is not recommended as it is better to be more specific and include both the slot number and the channel letter.

FlexRT Commands

Use these interpolation/range commands to apply selected channel overides to universal (shared) settings that configure how FlexRT interpolates and samples the channel waveform. The universal settings are made in the real-time scope's Scope Setup dialog or programmatically using the universal interpolation commands and universal range commands. To enable or disable the use of shared software clock recovery settings with the selected channel, use the :CHANnel:RTSCope:TRACk command.

Use these software CDR commands to apply selected channel overides to universal (shared) settings that configure how FlexRT applies software clock recovery on the waveform. The universal settings are made in the real-time scope's Scope Setup dialog or programmatically using the universal software clock recovery commands. To enable or disable the use of shared software clock recovery settings with the selected channel, use the :CHANnel:RTSCope:TRACk command.